DisplayPath Class¶
-
class
NXOpen.CAM.
DisplayPath
¶ Bases:
NXOpen.TaggedObject
Represents a display path Builder
This is an abstract class and cannot be instantiated.
New in version NX7.5.0.
Properties¶
Property | Description |
---|---|
PathDisplayType | Returns or sets the path display types |
ReplaySpeed | Returns or sets the replay speed. |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
DisplayPathPathDisplayTypes Enumeration | the path display types |
Property Detail¶
PathDisplayType¶
-
DisplayPath.
PathDisplayType
¶ Returns or sets the path display types
-------------------------------------
Getter Method
Signature
PathDisplayType
Returns: the path display type Return type: NXOpen.CAM.DisplayPathPathDisplayTypes
New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PathDisplayType
Parameters: pathDisplay ( NXOpen.CAM.DisplayPathPathDisplayTypes
) – the path display typeNew in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)
ReplaySpeed¶
-
DisplayPath.
ReplaySpeed
¶ Returns or sets the replay speed.
The range is 1-10.
-------------------------------------
Getter Method
Signature
ReplaySpeed
Returns: the replay speed. The range is 1-10. Return type: int New in version NX7.5.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ReplaySpeed
Parameters: displaySpeed (int) – the replay speed. The range is 1-10. New in version NX7.5.0.
License requirements: cam_base (“CAM BASE”)