CutterExportHolderExportStatus Enumeration¶
NXOpen.CAM.CutterExport.HolderExportStatus is an alias for NXOpen.CAM.CutterExportHolderExportStatus
-
class
NXOpen.CAM.
CutterExportHolderExportStatus
¶ Bases:
object
the holder export status
Enum Members
Enum Member Enum Member Description Ok Holder has been export successfully Unchanged Holder in library unchanged Undefined Holder is not defined Untried Holder export didn’t happen Fail Holder export failed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-