CutVolumeGeom Class¶
-
class
NXOpen.CAM.
CutVolumeGeom
¶ Bases:
NXOpen.TaggedObject
The classs represent the builder for creating cut volume features
New in version NX8.0.0.
Properties¶
Property | Description |
---|---|
CutVolumes | Returns the features |
Selection | Returns the selection |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
CreateCutVolume | Create an empty cut volume |
Property Detail¶
CutVolumes¶
-
CutVolumeGeom.
CutVolumes
¶ Returns the features
-------------------------------------
Getter Method
Signature
CutVolumes
Returns: Return type: NXOpen.CAM.CutVolumeList
New in version NX8.0.0.
License requirements: None.
Selection¶
-
CutVolumeGeom.
Selection
¶ Returns the selection
-------------------------------------
Getter Method
Signature
Selection
Returns: Return type: NXOpen.CAM.SelectCAMFeature
New in version NX8.0.0.
License requirements: None.
Method Detail¶
CreateCutVolume¶
-
CutVolumeGeom.
CreateCutVolume
¶ Create an empty cut volume
Signature
CreateCutVolume()
Returns: the cut volume feature object Return type: NXOpen.CAM.CutVolume
New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)