CutStrategyTypes Enumeration¶
NXOpen.CAM.CutStrategy.Types is an alias for NXOpen.CAM.CutStrategyTypes
-
class
NXOpen.CAM.
CutStrategyTypes
¶ Bases:
object
The cut strategy options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description LevelZ Cut strategy: Level Zig LevelZz Cut strategy: Level Zig-Zag RampingZ Cut strategy: Ramping Zig RampingZz Cut strategy: Ramping Zig-Zag ContourZ Cut strategy: Contour Zig ContourZz Cut strategy: Ramping Zig-Zag PlungeZ Cut strategy: Plunge Zig PlungeZz Cut strategy: Plunge Zig-Zag PlungeAlt Cut strategy: Plunge Alternate PlungeCastleing Cut strategy: Plunge Castleing PartOff Cut strategy: Part Off BlankContourZ Cut strategy: Blank Contour Zig -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-