CutSidesSideType Enumeration

NXOpen.CAM.CutSides.SideType is an alias for NXOpen.CAM.CutSidesSideType

class NXOpen.CAM.CutSidesSideType

Bases: object

Available types for sides to cut

Enum Members

Enum Member Enum Member Description
All All Sides
Left Left Side
Right Right Side
LeftRight Left and Right Side
Opposing Opposing Sides
LeftRightLeadingEdge Left, Right, Leading Edge
LeadingEdge Leading Edge
TrailingEdge Trailing Edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.