CutSideBuilder Class¶
-
class
NXOpen.CAM.
CutSideBuilder
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a cut side builder
This is an abstract class and cannot be instantiated.
New in version NX11.0.2.
Properties¶
Property | Description |
---|---|
CutSide | Returns or sets the cut side used for common block |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CutSideBuilderOption Enumeration | Enum of cut side |
Property Detail¶
CutSide¶
-
CutSideBuilder.
CutSide
¶ Returns or sets the cut side used for common block
-------------------------------------
Getter Method
Signature
CutSide
Returns: the cut side value Return type: NXOpen.CAM.CutSideBuilderOption
New in version NX11.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutSide
Parameters: cutSide ( NXOpen.CAM.CutSideBuilderOption
) – the cut side valueNew in version NX11.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
CutSideBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.