CutPatternBuilderTypes Enumeration¶
NXOpen.CAM.CutPatternBuilder.Types is an alias for NXOpen.CAM.CutPatternBuilderTypes
-
class
NXOpen.CAM.
CutPatternBuilderTypes
¶ Bases:
object
cut pattern options
New in version NX6.0.0.
Enum Members
Enum Member Enum Member Description NotSet None FollowPart Follow Part FollowPeriphery Follow Periphery Helical Helical Spiral Spiral HelicalSpiral Helical or Spiral Mixed Mixed Profile Profile StandardDrive Standard Drive Trochoidal Trochoidal Zig Zig ZigZag Zig Zag ZigZagWithLifts Zig Zag with Lifts ZigWithContour Zig with Contour ZigWithStepover Zig with Stepover ConcentricZig Concentric Zig ConcentricZigZag Concentric Zig Zag ConcentricZigWithContour Concentric Zig with Contour ConcentricZigWithStepover Concentric Zig with Stepover RadialZig Radial Zig RadialZigZag Radial Zig Zag RadialZigZagWithLifts Radial Zig Zag with Lifts RadialZigWithContour Radial Zig with Contour RadialZigWithStepover Radial Zig with Stepover CrosscutZig Crosscut Zig CrosscutZigZag Crosscut Zig Zag CrosscutZigZagWithLifts Crosscut Zig Zag with Lifts ZlevelZig Zlevel Zig ZlevelZigZag Zlevel Zig Zag ZlevelZigZagWithLifts Zlevel Zig Zag with Lifts SameAsNonSteep Same as Non-steep AdaptiveZig Adaptive Zig HelicalAroundPart Helical Around Part AdaptiveRoughing Adaptive Roughing ZlevelHelical Zlevel Helical -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-