CutLevelPlanarTypes Enumeration¶
NXOpen.CAM.CutLevelPlanar.Types is an alias for NXOpen.CAM.CutLevelPlanarTypes
-
class
NXOpen.CAM.
CutLevelPlanarTypes
¶ Bases:
object
cut level types
New in version NX7.5.0.
Enum Members
Enum Member Enum Member Description UserDefined User Defined FloorOnly Floor Only FloorAndCriticalDepth Floor, Then Critical Depths CriticalDepth Critical Depths Constant Constant -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-