CutBandTypes Enumeration

NXOpen.CAM.CutBand.Types is an alias for NXOpen.CAM.CutBandTypes

class NXOpen.CAM.CutBandTypes

Bases: object

Available types for Cut Band

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Offsets Offsets
Stepovers Stepovers
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.