CustomLoopSet Class¶
-
class
NXOpen.CAM.
CustomLoopSet
¶ Bases:
NXOpen.TaggedObject
,NXOpen.GeometricUtilities.IComponentBuilder
Represents a loop set object
To create a new instance of this class, use
NXOpen.CAM.CustomLoops.CreateLoopSet()
New in version NX8.0.0.
Deprecated since version NX9.0.0: Use
NXOpen.Features.PatchOpeningsBuilder
instead.
Properties¶
Property | Description |
---|---|
Ignored | Returns or sets the ignored status |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Ignored¶
-
CustomLoopSet.
Ignored
¶ Returns or sets the ignored status
-------------------------------------
Getter Method
Signature
Ignored
Returns: the ignore status Return type: bool New in version NX8.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Ignored
Parameters: isIgnored (bool) – the ignore status New in version NX8.0.0.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
CustomLoopSet.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.