ConvertFromMCDBuilderPocketLocationTypes Enumeration

NXOpen.CAM.ConvertFromMCDBuilder.PocketLocationTypes is an alias for NXOpen.CAM.ConvertFromMCDBuilderPocketLocationTypes

class NXOpen.CAM.ConvertFromMCDBuilderPocketLocationTypes

Bases: object

Represents the pocket location option.

Enum Members

Enum Member Enum Member Description
Spindle
ToolMagazine
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.