ConvertFromMCDBuilderMachineTypes Enumeration

NXOpen.CAM.ConvertFromMCDBuilder.MachineTypes is an alias for NXOpen.CAM.ConvertFromMCDBuilderMachineTypes

class NXOpen.CAM.ConvertFromMCDBuilderMachineTypes

Bases: object

Represents the machine type option.

Enum Members

Enum Member Enum Member Description
Mill
Turn
MillTurn
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.