CleanupOutputGeomTypes Enumeration

NXOpen.CAM.CleanupOutput.GeomTypes is an alias for NXOpen.CAM.CleanupOutputGeomTypes

class NXOpen.CAM.CleanupOutputGeomTypes

Bases: object

Available types for cleanup outputing geometry type, Cleanup Geometry Output

Enum Members

Enum Member Enum Member Description
Point Points
Bnd Boundaries
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.