CircularAboutAxisMoveBuilder Class¶
-
class
NXOpen.CAM.
CircularAboutAxisMoveBuilder
¶ Bases:
NXOpen.CAM.MoveBuilder
Represents the Circular Move To Point Builder
To create a new instance of this class, use
NXOpen.CAM.MoveCollection.CreateCircularAboutAxisMoveBuilder()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
ArcAxis | Returns or sets the arc axis |
ArcAxisType | Returns or sets the axis type |
ArcExtendMethod | Returns or sets the arc extension type |
CenterPoint | Returns or sets the center |
EndPoint | Returns or sets the arc end point |
ExtendAngle | Returns or sets the extend angle |
ExtendDistance | Returns or sets the extend distance |
FeedRate | Returns or sets the feed rate |
FeedType | Returns or sets the feed type |
FeedUnit | Returns or sets the feed unit |
MotionEndType | Returns or sets the arc end type |
MotionType | Returns or sets the motion type |
NumberOfUserParameters | Returns the number of user parameters |
ProtectedMove | Returns or sets the protected move status |
SubopLabel | Returns or sets the subop label |
SweepAngle | Returns or sets the sweep angle |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
GetUserParameter | Returns the custom parameter with the given name. |
SetParent | Set parent |
SetSibling | Set sibling |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
CircularAboutAxisMoveBuilderAxisType Enumeration | the axis type |
CircularAboutAxisMoveBuilderEndType Enumeration | the motion end type |
CircularAboutAxisMoveBuilderExtensionType Enumeration | the extension type |
Property Detail¶
ArcAxis¶
-
CircularAboutAxisMoveBuilder.
ArcAxis
¶ Returns or sets the arc axis
-------------------------------------
Getter Method
Signature
ArcAxis
Returns: Return type: NXOpen.Direction
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcAxis
Parameters: vec ( NXOpen.Direction
) –New in version NX5.0.0.
License requirements: None.
ArcAxisType¶
-
CircularAboutAxisMoveBuilder.
ArcAxisType
¶ Returns or sets the axis type
-------------------------------------
Getter Method
Signature
ArcAxisType
Returns: Return type: NXOpen.CAM.CircularAboutAxisMoveBuilderAxisType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcAxisType
Parameters: axisType ( NXOpen.CAM.CircularAboutAxisMoveBuilderAxisType
) –New in version NX5.0.0.
License requirements: None.
ArcExtendMethod¶
-
CircularAboutAxisMoveBuilder.
ArcExtendMethod
¶ Returns or sets the arc extension type
-------------------------------------
Getter Method
Signature
ArcExtendMethod
Returns: Return type: NXOpen.CAM.CircularAboutAxisMoveBuilderExtensionType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ArcExtendMethod
Parameters: arcExtendMethod ( NXOpen.CAM.CircularAboutAxisMoveBuilderExtensionType
) –New in version NX5.0.0.
License requirements: None.
CenterPoint¶
-
CircularAboutAxisMoveBuilder.
CenterPoint
¶ Returns or sets the center
-------------------------------------
Getter Method
Signature
CenterPoint
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CenterPoint
Parameters: location ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
EndPoint¶
-
CircularAboutAxisMoveBuilder.
EndPoint
¶ Returns or sets the arc end point
-------------------------------------
Getter Method
Signature
EndPoint
Returns: Return type: NXOpen.Point
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
EndPoint
Parameters: location ( NXOpen.Point
) –New in version NX5.0.0.
License requirements: None.
ExtendAngle¶
-
CircularAboutAxisMoveBuilder.
ExtendAngle
¶ Returns or sets the extend angle
-------------------------------------
Getter Method
Signature
ExtendAngle
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendAngle
Parameters: extendAngle (float) – New in version NX5.0.0.
License requirements: None.
ExtendDistance¶
-
CircularAboutAxisMoveBuilder.
ExtendDistance
¶ Returns or sets the extend distance
-------------------------------------
Getter Method
Signature
ExtendDistance
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ExtendDistance
Parameters: extendDistance (float) – New in version NX5.0.0.
License requirements: None.
MotionEndType¶
-
CircularAboutAxisMoveBuilder.
MotionEndType
¶ Returns or sets the arc end type
-------------------------------------
Getter Method
Signature
MotionEndType
Returns: Return type: NXOpen.CAM.CircularAboutAxisMoveBuilderEndType
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
MotionEndType
Parameters: arcEndType ( NXOpen.CAM.CircularAboutAxisMoveBuilderEndType
) –New in version NX5.0.0.
License requirements: None.
SweepAngle¶
-
CircularAboutAxisMoveBuilder.
SweepAngle
¶ Returns or sets the sweep angle
-------------------------------------
Getter Method
Signature
SweepAngle
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SweepAngle
Parameters: sweepAngle (float) – New in version NX5.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
CircularAboutAxisMoveBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.