ChamferMillingBuilder Class¶
-
class
NXOpen.CAM.
ChamferMillingBuilder
¶ Bases:
NXOpen.CAM.HoleMachiningBuilder
Represents a ChamferMillingBuilder Builder
To create a new instance of this class, use
NXOpen.CAM.OperationCollection.CreateChamferMillingBuilder()
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
ChamferOffset | Returns or sets the chamfer offset |
ChamferReference | Returns or sets the chamfer reference |
ChannelName | Returns or sets the channel’s name |
CollisionCheck | Returns or sets the collision check for cutting |
CutParameters | Returns the Chamfer Milling Cut Parameters |
CuttingParameters | Returns the Cut Parameters |
CycleEvent | Returns the cycle event |
CycleTable | Returns the cycle |
Description | Returns or sets the description |
DrivePoint | Returns or sets the drive point |
EndOfPath | Returns the end event builder |
EndUdeSet | Returns the end ude set |
FeedsBuilder | Returns the feeds and speeds builder |
Geometry | Returns the geometry builder |
GougeChecking | Returns or sets the gouge checking flag |
HoleAxisType | Returns or sets the Hole Axis Type |
HoleDepth | Returns the max depth distance builder |
HoleDepthType | Returns or sets the Hole Depth Type |
LayoutAndLayer | Returns the Layer and Layout |
MotionOutputBuilder | Returns the motion output builder |
NonCuttingBuilder | Returns the non-cutting moves builder |
Notes | Returns the notes builder |
OptimizationBasedOn | Returns or sets the optimization based on in operation |
OptimizationDistanceMethod | Returns or sets the optimization distance method in operation |
OptimizationLevel | Returns or sets the optimization level in operation |
OptimizationMethod | Returns or sets the optim method |
PathDisplayOptions | Returns the path display options builder |
PostToolPathExit | Returns or sets the environment variable that points to the post tool path generation library which has the exit |
PredefinedDepth | Returns the predefined depth |
RetractDistance | Returns the Retract Distance builder (inheritable double) |
RetractDistanceOnToolAxisChange | Returns the Retract Distance on Tool Axis Change builder (inheritable double) |
SafeClearance | Returns the safe clearance builder |
SelectToolFlag | Returns or sets the user selected tool |
StartOfPath | Returns the start event builder |
StartUdeSet | Returns the start ude set |
Tag | Returns the Tag for this object. |
ToolChangeSetting | Returns the tool change builder |
ToolPathEditor | Returns the Tool Path Editor Builder |
ToolPathSplitParametersBuilder | Returns the tool path split Parameters |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetCustomizableItemBuilder | Returns the customizable item builder for the given customizable item name |
GetCustomizableItemNames | Returns the names for all customizable item ids |
GetFeatureGeometry | Returns the feature geometry |
GetHoleAxisValues | Get the Hole Axis values |
GetObject | Returns the object currently being edited by this builder. |
RemoveOverrides | Removes overridden attributes of features in the feature geometry |
SetHoleAxisValues | Set the Hole Axis values |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnlockFeatures | Unlocks locked features in the feature geometry |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
ChamferMillingBuilderChamferReferenceType Enumeration | Available types for chamfer reference |
Property Detail¶
ChamferOffset¶
-
ChamferMillingBuilder.
ChamferOffset
¶ Returns or sets the chamfer offset
-------------------------------------
Getter Method
Signature
ChamferOffset
Returns: the chamfer offset Return type: float New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChamferOffset
Parameters: chamferOffsetValue (float) – the chamfer offset New in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
ChamferReference¶
-
ChamferMillingBuilder.
ChamferReference
¶ Returns or sets the chamfer reference
-------------------------------------
Getter Method
Signature
ChamferReference
Returns: The chamfer reference type Return type: NXOpen.CAM.ChamferMillingBuilderChamferReferenceType
New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ChamferReference
Parameters: chamferReference ( NXOpen.CAM.ChamferMillingBuilderChamferReferenceType
) – The chamfer reference typeNew in version NX11.0.0.
License requirements: cam_base (“CAM BASE”)
CutParameters¶
-
ChamferMillingBuilder.
CutParameters
¶ Returns the Chamfer Milling Cut Parameters
-------------------------------------
Getter Method
Signature
CutParameters
Returns: the Chamfer Milling Cut Parameters Return type: NXOpen.CAM.FeatureMillingCutParameters
New in version NX9.0.2.
Deprecated since version NX9.0.3: Use
CAM.HoleMachiningBuilder.CuttingParameters()
instead.License requirements: None.
DrivePoint¶
-
ChamferMillingBuilder.
DrivePoint
¶ Returns or sets the drive point
-------------------------------------
Getter Method
Signature
DrivePoint
Returns: The drive point name Return type: str New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
DrivePoint
Parameters: drivePoint (str) – The drive point name New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
ChamferMillingBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.