CamInspectionOperationFeaturetypes Enumeration¶
-
class
NXOpen.CAM.
CamInspectionOperationFeaturetypes
¶ Bases:
object
Specifies the type of an inspection feature Enum Members
Enum Member Enum Member Description NotSet Not a Feature Arc Arc Circle Circle Point Point Sphere Sphere Surface Surface Pattern Pattern Curve Curve Cylinder Cylinder Cone Cone Plane Plane Line Line Cparln Closed Parallel Line bounded slot SlotTab Slot or Tab SurfaceOfRevolution Surface of Revolution Torus Torus EdgePoint Edge Point -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-