CAMSetupPostprocessSettingsReviewTool Enumeration¶
NXOpen.CAM.CAMSetup.PostprocessSettingsReviewTool is an alias for NXOpen.CAM.CAMSetupPostprocessSettingsReviewTool
-
class
NXOpen.CAM.
CAMSetupPostprocessSettingsReviewTool
¶ Bases:
object
Review tool setting for Postprocess
Enum Members
Enum Member Enum Member Description On show the review tool window Off not show the review tool window PostDefined use post defined setting -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-