CAMSetupPaste Enumeration¶
NXOpen.CAM.CAMSetup.Paste is an alias for NXOpen.CAM.CAMSetupPaste
-
class
NXOpen.CAM.
CAMSetupPaste
¶ Bases:
object
Paste position.
Enum Members
Enum Member Enum Member Description Before paste before Inside paste inside After paste after -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-