CAMAttributeValueType Enumeration

NXOpen.CAM.CAMAttribute.ValueType is an alias for NXOpen.CAM.CAMAttributeValueType

class NXOpen.CAM.CAMAttributeValueType

Bases: object

Attribute types

Enum Members

Enum Member Enum Member Description
Integer
Double
String
Bool
Point3
Vector3
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.