BoundaryTurnMemberSetConcaveCornersTypeValue Enumeration

NXOpen.CAM.BoundaryTurnMemberSet.ConcaveCornersTypeValue is an alias for NXOpen.CAM.BoundaryTurnMemberSetConcaveCornersTypeValue

class NXOpen.CAM.BoundaryTurnMemberSetConcaveCornersTypeValue

Bases: object

the types available for the concave corners

Enum Members

Enum Member Enum Member Description
Extend
ConnectLinear
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.