BoundaryTurnMemberOffsetDistanceTypeMode Enumeration

NXOpen.CAM.BoundaryTurnMemberOffset.DistanceTypeMode is an alias for NXOpen.CAM.BoundaryTurnMemberOffsetDistanceTypeMode

class NXOpen.CAM.BoundaryTurnMemberOffsetDistanceTypeMode

Bases: object

the types available for member distance

Enum Members

Enum Member Enum Member Description
Nominal
Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.