BoundaryTurnMemberFineFinishOffsetTypeValue Enumeration

NXOpen.CAM.BoundaryTurnMemberFineFinishOffset.TypeValue is an alias for NXOpen.CAM.BoundaryTurnMemberFineFinishOffsetTypeValue

class NXOpen.CAM.BoundaryTurnMemberFineFinishOffsetTypeValue

Bases: object

the types available for fine finsish offset method

Enum Members

Enum Member Enum Member Description
Nominal
Diameter
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.