BoundaryTurnMemberFineFinishOffsetStatusValue Enumeration

NXOpen.CAM.BoundaryTurnMemberFineFinishOffset.StatusValue is an alias for NXOpen.CAM.BoundaryTurnMemberFineFinishOffsetStatusValue

class NXOpen.CAM.BoundaryTurnMemberFineFinishOffsetStatusValue

Bases: object

the fine finish offset stati available

Enum Members

Enum Member Enum Member Description
NotSet
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.