BoundaryTurnMemberFeed Class¶
-
class
NXOpen.CAM.
BoundaryTurnMemberFeed
¶ Bases:
NXOpen.Builder
Represents a
NXOpen.CAM.BoundaryTurnMemberFeed
This builder cannot be instantiated separately.
New in version NX9.0.2.
Properties¶
Property | Description |
---|---|
CustomFeedType | Returns or sets the corner feed rate type |
FeedUnit | Returns or sets the feed rate unit |
FeedValue | Returns or sets the feed rate value |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
BoundaryTurnMemberFeedFeedType Enumeration | the corner feed rate types available |
Property Detail¶
CustomFeedType¶
-
BoundaryTurnMemberFeed.
CustomFeedType
¶ Returns or sets the corner feed rate type
-------------------------------------
Getter Method
Signature
CustomFeedType
Returns: Return type: NXOpen.CAM.BoundaryTurnMemberFeedFeedType
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
CustomFeedType
Parameters: newValue ( NXOpen.CAM.BoundaryTurnMemberFeedFeedType
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FeedUnit¶
-
BoundaryTurnMemberFeed.
FeedUnit
¶ Returns or sets the feed rate unit
-------------------------------------
Getter Method
Signature
FeedUnit
Returns: Return type: NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedUnit
Parameters: newUnit ( NXOpen.CAM.BoundaryTurnSetFeedUnitTypes
) –New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
FeedValue¶
-
BoundaryTurnMemberFeed.
FeedValue
¶ Returns or sets the feed rate value
-------------------------------------
Getter Method
Signature
FeedValue
Returns: Return type: float New in version NX9.0.2.
License requirements: None.
-------------------------------------
Setter Method
Signature
FeedValue
Parameters: newValue (float) – New in version NX9.0.2.
License requirements: cam_base (“CAM BASE”)
Method Detail¶
Validate¶
-
BoundaryTurnMemberFeed.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.