BoundaryTurnMemberCornerFeedType Enumeration

NXOpen.CAM.BoundaryTurnMemberCorner.FeedType is an alias for NXOpen.CAM.BoundaryTurnMemberCornerFeedType

class NXOpen.CAM.BoundaryTurnMemberCornerFeedType

Bases: object

the corner feed rate types available

Enum Members

Enum Member Enum Member Description
NotSet
Specify
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.