BoundaryTurnMemberCornerCornerType Enumeration

NXOpen.CAM.BoundaryTurnMemberCorner.CornerType is an alias for NXOpen.CAM.BoundaryTurnMemberCornerCornerType

class NXOpen.CAM.BoundaryTurnMemberCornerCornerType

Bases: object

the corner types available

Enum Members

Enum Member Enum Member Description
General
ConstantRadiusChamfer
KeepTangentPoint
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.