BoundaryTurnMemberCornerAngleValueType Enumeration

NXOpen.CAM.BoundaryTurnMemberCorner.AngleValueType is an alias for NXOpen.CAM.BoundaryTurnMemberCornerAngleValueType

class NXOpen.CAM.BoundaryTurnMemberCornerAngleValueType

Bases: object

the corner angle types available

Enum Members

Enum Member Enum Member Description
NotSet
Currentsegment
Previoussegment
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.