BoundaryTurnBlankPosition Enumeration

NXOpen.CAM.BoundaryTurnBlank.Position is an alias for NXOpen.CAM.BoundaryTurnBlankPosition

class NXOpen.CAM.BoundaryTurnBlankPosition

Bases: object

the mounting direction types available

Enum Members

Enum Member Enum Member Description
AtHeadstock
AwayfromHeadstock
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.