BoundaryPlanarMill Class¶
-
class
NXOpen.CAM.
BoundaryPlanarMill
¶ Bases:
NXOpen.CAM.Boundary
Represents a CAM boundary object
This is an abstract class and cannot be instantiated.
New in version NX11.0.1.
Properties¶
Property | Description |
---|---|
BoundaryList | Returns the boundary list |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
AppendFaceBoundary | Append the face boundary |
CreateBoundaryMillingSet | Create an empty milling boundary set |
CreateBoundarySet | Create an empty boundary set |
CreateBoundarySetPlanarMill | Create an empty boundary set for planar mill/surface contour operation |
CreateBoundaryTurnSet | Create an empty turning boundary set |
RemoveFaceBoundary | Remove the face boundaries |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Method Detail¶
AppendFaceBoundary¶
-
BoundaryPlanarMill.
AppendFaceBoundary
¶ Overloaded method AppendFaceBoundary
AppendFaceBoundary(face, ignoreHole, ignoreIsland, ignoreChamfer, toolSide, convexEdges, concaveEdges)
AppendFaceBoundary(face, ignoreHole, ignoreIsland, ignoreChamfer, toolSide)
-------------------------------------
Append the face boundary
Signature
AppendFaceBoundary(face, ignoreHole, ignoreIsland, ignoreChamfer, toolSide, convexEdges, concaveEdges)
Parameters: - face (
NXOpen.TaggedObject
) – the face to create boundaries - ignoreHole (bool) – flag to ignore holes in face
- ignoreIsland (bool) – flag to ignore islands on face
- ignoreChamfer (bool) – flag to ignore chamfers on face
- toolSide (
NXOpen.CAM.BoundarySetToolSideTypes
) – tool side for the face boundary - convexEdges (int) – the tool position type for convex edges
- concaveEdges (int) – the tool position type for concave edges
Returns: array of the appended face boundary set objects
Return type: list of
NXOpen.CAM.BoundarySet
New in version NX11.0.1.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Append the face boundary
Signature
AppendFaceBoundary(face, ignoreHole, ignoreIsland, ignoreChamfer, toolSide)
Parameters: - face (
NXOpen.TaggedObject
) – the face to create boundaries - ignoreHole (bool) – flag to ignore holes in face
- ignoreIsland (bool) – flag to ignore islands on face
- ignoreChamfer (bool) – flag to ignore chamfers on face
- toolSide (
NXOpen.CAM.BoundarySetToolSideTypes
) – tool side for the face boundary
Returns: array of the appended face boundary set objects
Return type: list of
NXOpen.CAM.BoundarySet
New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
-------------------------------------
Validate¶
-
BoundaryPlanarMill.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.