BlankIpwStatusTypes Enumeration¶
NXOpen.CAM.BlankIpw.StatusTypes is an alias for NXOpen.CAM.BlankIpwStatusTypes
-
class
NXOpen.CAM.
BlankIpwStatusTypes
¶ Bases:
object
the blank IPW status types
Enum Members
Enum Member Enum Member Description UpToDate blank ipw status up to date OutOfDate blank ipw status out of date UnableToUpdate blank ipw status unable to update NotSet blank ipw status none Unknown blank ipw status unknown -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-