BladeStartPointTypes Enumeration

NXOpen.CAM.BladeStartPoint.Types is an alias for NXOpen.CAM.BladeStartPointTypes

class NXOpen.CAM.BladeStartPointTypes

Bases: object

Available types for Blade Start Point

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
LeadingEdge Leading Edge
TrailingEdge Trailing Edge
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.