BladeFinishGeomTypes Enumeration

NXOpen.CAM.BladeFinishGeom.Types is an alias for NXOpen.CAM.BladeFinishGeomTypes

class NXOpen.CAM.BladeFinishGeomTypes

Bases: object

Available types for geometry to finish

Enum Members

Enum Member Enum Member Description
Blade Blade
SplitterOne Splitter 1
SplitterTwo Splitter 2
SplitterThree Splitter 3
SplitterFour Splitter 4
SplitterFive Splitter 5
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.