BladeEdgeEdgePointType Enumeration

NXOpen.CAM.BladeEdge.EdgePointType is an alias for NXOpen.CAM.BladeEdgeEdgePointType

class NXOpen.CAM.BladeEdgeEdgePointType

Bases: object

Available types for Blade Edge Point

Enum Members

Enum Member Enum Member Description
AlongBladeDirection along blade direction
AlongPartAxis along part axis
NoCurling no curling
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.