AreaMillingSteepContainment Class¶
-
class
NXOpen.CAM.
AreaMillingSteepContainment
¶ Bases:
NXOpen.CAM.AreaMillingContainment
Represents a Steep Containment Builder
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
AreaMillingCutDirection | Returns or sets the Cut Direction |
CutLevelType | Returns or sets the cut level type |
CutPattern | Returns the cut pattern builder |
DepthPerCut | Returns the builder of area milling depth per cut |
Stepover | Returns the builder of area milling stepover |
Tag | Returns the Tag for this object. |
Methods¶
Enumerations¶
AreaMillingSteepContainmentCutLevelTypes Enumeration | cut level types |
Property Detail¶
AreaMillingCutDirection¶
-
AreaMillingSteepContainment.
AreaMillingCutDirection
¶ Returns or sets the Cut Direction
-------------------------------------
Getter Method
Signature
AreaMillingCutDirection
Returns: the Offset Mode value Return type: NXOpen.CAM.AreaMillingContainmentCutDirectionTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
AreaMillingCutDirection
Parameters: areaMillingCutDirection ( NXOpen.CAM.AreaMillingContainmentCutDirectionTypes
) – the Offset Mode valueNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
CutLevelType¶
-
AreaMillingSteepContainment.
CutLevelType
¶ Returns or sets the cut level type
-------------------------------------
Getter Method
Signature
CutLevelType
Returns: the cut level type Return type: NXOpen.CAM.AreaMillingSteepContainmentCutLevelTypes
New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CutLevelType
Parameters: newValue ( NXOpen.CAM.AreaMillingSteepContainmentCutLevelTypes
) – the cut level typeNew in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
DepthPerCut¶
-
AreaMillingSteepContainment.
DepthPerCut
¶ Returns the builder of area milling depth per cut
-------------------------------------
Getter Method
Signature
DepthPerCut
Returns: The depth per cut builder Return type: NXOpen.CAM.StepoverBuilder
New in version NX9.0.0.
License requirements: None.