WindowManager Class¶
-
class
NXOpen.CAE.Xyplot.
WindowManager
¶ Bases:
object
Manages the separate graphic windows.
The value of device index is greater than 0. This class is restricted to being called from a program running during an interactive NX session. If run from a non-interactive session it will return None. To obtain an instance of this class use
NXOpen.CAE.Xyplot.XYPlotManager.WindowManager()
.New in version NX9.0.0.
Methods¶
Method | Description |
---|---|
CloseWindow | Closes the window of specified device index. |
GetWindows | Gets the device indices of all the graphic windows. |
NewWindow | Creates a new window and returns the device index. |
Method Detail¶
CloseWindow¶
-
WindowManager.
CloseWindow
¶ Closes the window of specified device index.
Signature
CloseWindow(deviceIndex)
Parameters: deviceIndex (int) – New in version NX9.0.0.
License requirements: None.