PreferenceTargetGraphicWindowOption Enumeration¶
NXOpen.CAE.Xyplot.Preference.TargetGraphicWindowOption is an alias for NXOpen.CAE.Xyplot.PreferenceTargetGraphicWindowOption
-
class
NXOpen.CAE.Xyplot.
PreferenceTargetGraphicWindowOption
¶ Bases:
object
Defines the target graphic window type
Enum Members
Enum Member Enum Member Description Main Only shows plot graph on main graphic window Separate Only shows plot graph on a separate graphic window Both Shows plot graph on either main graphic window or a separate graphic window -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-