PlotParameters Class¶
-
class
NXOpen.CAE.Xyplot.
PlotParameters
¶ Bases:
NXOpen.CAE.Xyplot.BasePlotParameters
Represents the parameters passed to create a plot.
To create a new instance of this class, use
NXOpen.CAE.Xyplot.XYPlotManager.NewPlotParameters()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
ComplexOption | Returns or sets the complex options,if complex option is smaller than zero, it will use default complex option from active template file |
DeviceIndex | Returns or sets the index of device on which plot graph will be shown. |
IsToCreateStandalonePlot | Returns or sets the create standalone plot |
PlotTemplate | Returns the plot template to be used by the plot |
PlotType | Returns or sets the plot type |
ViewPortIndex | Returns or sets the index of a view port on main graphic window, on which plot graph will be shown. |
Methods¶
Method | Description |
---|---|
Dispose | Destroys the object |
GetRecords | Gets the records to be plotted |
SetRecords | Sets the records to be plotted |
Property Detail¶
ComplexOption¶
-
PlotParameters.
ComplexOption
¶ Returns or sets the complex options,if complex option is smaller than zero, it will use default complex option from active template file
-------------------------------------
Getter Method
Signature
ComplexOption
Returns: Return type: int New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
ComplexOption
Parameters: complexOption (int) – New in version NX11.0.0.
License requirements: None.
IsToCreateStandalonePlot¶
-
PlotParameters.
IsToCreateStandalonePlot
¶ Returns or sets the create standalone plot
-------------------------------------
Getter Method
Signature
IsToCreateStandalonePlot
Returns: Return type: bool New in version NX11.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
IsToCreateStandalonePlot
Parameters: isToCreateStandalonePlot (bool) – New in version NX11.0.0.
License requirements: None.
PlotTemplate¶
-
PlotParameters.
PlotTemplate
¶ Returns the plot template to be used by the plot
-------------------------------------
Getter Method
Signature
PlotTemplate
Returns: Return type: NXOpen.CAE.Xyplot.PlotGraphTemplate
New in version NX10.0.0.
License requirements: None.
PlotType¶
-
PlotParameters.
PlotType
¶ Returns or sets the plot type
-------------------------------------
Getter Method
Signature
PlotType
Returns: Return type: NXOpen.CAE.Xyplot.PlotType
New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
PlotType
Parameters: plotType ( NXOpen.CAE.Xyplot.PlotType
) –New in version NX10.0.0.
License requirements: None.