ModelType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
ModelType
¶ Bases:
object
Represents the model type Enum Members
Enum Member Enum Member Description Plot Graph RecordDisplay Marker Note Title GraphName FunctionName the lable of a record for CAE.XyplotPlotType.PlotColorBar
XAxis XAxisLabel XAxisNumber YAxis YAxisLabel YAxisNumber ZAxis ZAxisLabel ZAxisNumber ColorAxis the color indicator for CAE.XyplotPlotType.PlotColorBar
andCAE.XyplotPlotType.PlotColorMap
ColorAxisLabel ColorAxisNumber AngleAxis the axis to display angle divisions on circle grids AngleAxisNumber the angle axis number UnknownResult the label and color block to represent result value beyond color range on CAE.XyplotPlotType.PlotColorBar
andCAE.XyplotPlotType.PlotColorMap
PageNumber Legend LegendTable -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-