LimitsType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
LimitsType
¶ Bases:
object
Represents the axis limits type Enum Members
Enum Member Enum Member Description FreeLimits Type to use source data limits as axis limits OptimizedLimits Type to optimize source data limits to natural axis limits FixedLimits Type to use customized data limits as axis limits -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-