LegendTablePositionType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
LegendTablePositionType
¶ Bases:
object
Represents the legend table position type Enum Members
Enum Member Enum Member Description Floating The position of legend table can be dragged Docked The position of legend table is fixed -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-