GraphStyle Enumeration¶
-
class
NXOpen.CAE.Xyplot.
GraphStyle
¶ Bases:
object
Represents the plot graph style Enum Members
Enum Member Enum Member Description Line Option to display plot in curve style Bar Option to display plot in bar style Plate Deprecated in NX12.0 Surface Option to display plot in surface style Scatter Option to display plot in scatter style ColorBar Option to display plot in ColorBar style ColorMap Option to display plot in ColorMap style BarChart Option to display plot in BarChart style Vector Option to display plot in vector style -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-