Direction Enumeration¶
-
class
NXOpen.CAE.Xyplot.
Direction
¶ Bases:
object
Represents the direction option Enum Members
Enum Member Enum Member Description X Option to show plot in the X axis direction Z Option to show plot in the Z axis direction Xz Option to show plot in the both X and Z axis direction -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-