DecimalFormat Enumeration¶
-
class
NXOpen.CAE.Xyplot.
DecimalFormat
¶ Bases:
object
Represents the decimal number format Enum Members
Enum Member Enum Member Description Actual Show decimal automatically X Displays one digit followed by period Xx Displays two digits followed by period Xxx Displays three digits followed by period Xxxx Displays four digits followed by period Xexx Scientific notation with one digit followed by period,for example: 5.3E+05 Xxexx Scientific notation with two digits followed by period Xxxexx Scientific notation with three digits followed by period Xxxxexx Scientific notation with four digits followed by period -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-