CoordinateType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
CoordinateType
¶ Bases:
object
Represents the swap axis type Enum Members
Enum Member Enum Member Description Xy no swap for 2d Yx swap x and y Xyz no swap for 3d Yxz swap x and y Zyx swap x and z Yzx swap x and y firstly and then swap y and z Xzy swap Z and y Zxy swap x and y firstly and then swap X and z -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-