AxisType Enumeration¶
-
class
NXOpen.CAE.Xyplot.
AxisType
¶ Bases:
object
Represents the type of scale for X or Y axis Enum Members
Enum Member Enum Member Description Auto Automatic type Linear Linear type Log Log type Db Db type Octave Octave type OneThirdOctave 1/3 Octave type OneTwelfthOctave 1/12 Octave type -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-