XyFunctionMotionType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionMotionType
¶ Bases:
object
Defines motion purpose type of a function Enum Members
Enum Member Enum Member Description Time Function is Time History TimingChart Function is Timing Chart StiffnessAndDamping Function is Stiffness and Damping Vehicle Function is Vehicle MotionGeneral Function is Motion General Function Number Motion Type Function Number -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-