XyFunctionMeasure Enumeration¶
-
class
NXOpen.CAE.
XyFunctionMeasure
¶ Bases:
object
Defines measurement unit types Enum Members
Enum Member Enum Member Description General General unit Displacement Displacement unit Force Force unit Temperature Temperature unit Time Time unit Frequency Frequency unit Mass Mass unit Velocity Velocity unit Acceleration Acceleration unit AngularDisplacement Angular displacement unit AngularVelocity Angular velocity unit AngularAcceleration Angular acceleration unit Moment Moment unit Pressure Pressure unit Stress Stress unit Strain Strain unit Rpm RPM unit Order Order unit Cycles Cycles unit Loadfactor Load Factor unit Torque Torque unit Gravity Gravity unit Curvature Curvature unit ElementForce Element force unit ElementMoment Element moment unit MotorSignal Motor signal unit UnitlessScalar Unitless scalar unit UnitlessReal Unitless real unit UnitlessInteger Unitless integer unit Voltage Voltage unit ElectricCurrent Electric current unit Damping Damping Power Power MassFlow Mass flow Energy Energy Area Area MomentPerAngle Moment Per Angle DynamicViscosity Dynamic Viscosity ConvectionCoefficient Convection Coefficient HeatFlux Heat Flux VelocityPerPressure Velocity per Pressure MessDensity mess density SpecificHeat specific heat ThermalConductivity thermal conductivity ThermalExpansionCoefficient Thermal Expansion Coefficient LengthPerAngle Length Per Angle Number Measure number -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-