XyFunctionMaterialType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionMaterialType
¶ Bases:
object
Defines material purpose type of a function Enum Members
Enum Member Enum Member Description General Function is General Function. Time Function is Time History Temperature Function is Temperature StressStrain Function is Stress/Strain Function Life Function is Fatigue Life -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-