XyFunctionMacroType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionMacroType
¶ Bases:
object
Defines the application type of a function Enum Members
Enum Member Enum Member Description General Function could be used in any application Motion Function is only used in a motion application Response Function is only used to define a response Load Function is only used to define a load Material Function is only used to define a material -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-