XyFunctionGeneralType Enumeration¶
-
class
NXOpen.CAE.
XyFunctionGeneralType
¶ Bases:
object
Defines general purpose type of a function Enum Members
Enum Member Enum Member Description General Function is General Function. Time Function is Time History Spectrum Function is Spectrum PowerSpectralDensity Function is Power Spectral Density ShockResponseSpectrum Function is Shock Response Spectrum FrequencyResponseFunction Function is Frequency Response Function Temperature Function is Temperature StressStrain Function is Stress/Strain Function Life Function is Fatigue Life CrossSpectrum Function is Cross Spectrum Transmissibility Function is Transmissibility CampbellDiagram Function is Campbell Diagram TimingChart Function is Timing Chart StiffnessAndDamping Function is Stiffness and Damping FastRmsFittedPsd Function is Fast RMS Fitted PSD Vehicle Function is Vehicle MotionGeneral Function is Motion General Function Number General Type Function Number -
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-